High-Performance Mil-Spec and Commercial Contacts
Glenair brings a new perspective to the supply of high-performance Mil-Spec and commercial contacts: High Availability! Whether you need a standard duty socket for a MIL-DTL-28840 connector or an extended duty pin for MIL-DTL-38999 Series III, we have you covered with products that are always in stock — with no dollar or quantity minimums. In addition to the broadest selection and availability, Glenair also delivers outstanding interconnection compatibility. Glenair QPL SAE-AS39029 as well as our proprietary contact series are guaranteed to mate properly and perform at the upper limits of application requirements.
SAE AS39029 Crimp Contacts
In a marketplace saturated with specialty interconnection media, the SAE-AS39029 crimp contact is still the "bread and butter" of the circular connector world. Serving platforms like the D38999, M28840 and countless others, AS39029 crimp contacts continue to offer reliable power and signal transmission in ruggedized applications. A myriad of sizes, termination options and materials mean that end users don’t have to compromise performance or reliability.
High Performance Shielded Contacts
Glenair shielded contacts are fabricated from the best available materials and manufacturing processes. Conductive elements are gold-plated copper alloy. Dielectrics are high-performance fluorocarbon. When applicable, contacts are approved to SAE AS39029.
Fiber Optic Contacts
Today, the use of fiber optic systems to carry digitized video, voice and data is universal. High-performance fiber optic interconnect technologies, combined with satellite and other broadcast media, enable high-speed specialized applications in avionics, robotics, weapon systems, sensors, space and other high performance environments. Highly engineered fiber optic contacts, or termini, are the key to delivering low data loss and reliable, repeatable performance in fiber optic connection systems.
Our Series 80 Mighty Mouse Size #23 Crimp Contacts
Like all high-performance crimp contact systems, Series 80 Mighty Mouse contacts are terminated to wire using precision crimp tools, and are then snapped into place by hand or with a hand held insertion tool. Damaged or miswired contacts may be removed from the connector using special extraction tools. Although the connectors are supplied with a full complement of contacts, extra contacts are commonly purchased as spares or to use for quality assurance purposes, such as crimp tensile tests. Coaxial contacts are also typically ordered separately, as customers prefer to specify the exact performance values for these specialized shielded contacts.
Thermocouple and Other Special Purpose Contacts
Glenair produces a wide range of special purpose contacts including high power and high ampacity contacts, pneumatic contacts, PC Tail contacts for board terminations and thermocouple contacts for use in temperature measuring applications. We also produce all the small accessory items, such as sealing plugs, that make us a convenient one-stop-shopping destination for users of high-performance Mil-Spec and commercial connectors and contacts.
Crimp Contact Introductions
Slideshow Presentation
Glossary
Related Catalogs
- GT Pure Gas Tube Assemblies / Series 83
- Mighty Mouse — Micro Miniature Cylindrical Connectors and Cables for Harsh Sea, Air, Land, and Space Applications
We invite our customers to take advantage of the breadth and depth of our contact product line, especially in terms of its high-availability and our willingness to engineer unique and special-purpose contact solutions for virtually any interconnect challenge.
PC Tail Termination Note
To prevent detrimental intrusion of cleaning solvents/water into the connector when terminating, the connector must be protected IAW IPC J-STD-001 and/or NASA STD-8739.3. For assistance and/or additional information, please contact factory.
AS39029 QPL and Glenair Commercial High-Performance Connector Contacts
High-Performance Mil-Spec and Commercial Contacts
![]() |
SAE-AS39029 Crimp ContactsHigh Performance Pin and Socket Crimp Contacts Section A |
![]() |
QPL and Commercial High Performance Fiber Optic TerminiIndustry Leading Fiber Optic Technology Section C |
![]() |
Special Purpose High Performance ContactsThermocouple, Pneumatic, PC Tail, High Power, Solder Cup, and More Section D |
![]() |
Crimp Tools and AccessoriesCrimp Tools, Positioners, Insertion and Extraction Tools, and More Section E |